MAC_DRVR_Process Function

C

TCPIP_MAC_RES MAC_DRVR_Process( DRV_HANDLE hMac ); 

Returns

  • TCPIP_MAC_RES_OK if all processing went on OK
  • a TCPIP_MAC_RES error code if processing failed for some reason

Description

This is a function that allows for internal processing by the MAC driver. It is meant for processing that cannot be done from within ISR.

Normally this function will be called in response to an TX and/or RX event signaled by the driver. This is specified by the MAC driver at initialization time using TCPIP_MAC_MODULE_CTRL.

Remarks

  • The MAC driver may use the MAC_DRVR_Process() for:

    • Processing its pending TX queues
    • RX buffers replenishing functionality.

    If the number of packets in the RX queue falls below a specified limit, the MAC driver may use this function to allocate some extra RX packets. Similarly, if there are too many allocated RX packets, the MAC driver can free some of them.

Preconditions

  • MAC_DRVR_Initialize() should have been called.
  • MAC_DRVR_Open() should have been called to obtain a valid handle.

Parameters

ParametersDescription
hMacEthernet MAC client handle