MAC_DRVR_EventPendingGet Function

C

TCPIP_MAC_EVENT MAC_DRVR_EventPendingGet( DRV_HANDLE hMac );

Returns

The currently stack pending events.

Description

This function returns the currently pending Ethernet MAC events. Multiple events will be ORed together as they accumulate. The stack should perform processing whenever a transmission related event such as TCPIP_MAC_EV_RX_PKTPEND, or TCPIP_MAC_EV_TX_DONE, is present. The other, non critical events, may not be managed by the stack and passed to a user. They will have to be eventually acknowledged if re-enabling is needed.

Remarks

  • This is the preferred method to get the current pending MAC events. The stack maintains a proper image of the events from their occurrence to their acknowledgment.

  • Even with a notification handler in place it's better to use this function to get the current pending events rather than using the events passed by the notification handler which could be stale.

  • The events are persistent. They shouldn't be re-enabled unless they have been processed and the condition that generated them was removed. Re-enabling them immediately without proper processing will have dramatic effects on system performance.

  • The returned value is just a momentary value. The pending events can change any time.

Preconditions

  • MAC_DRVR_Initialize() should have been called.
  • MAC_DRVR_Open() should have been called to obtain a valid handle.

Parameters

ParametersDescription
hMacParameter identifying the intended MAC client