MAC_DRVR_LinkCheck Function

C

bool MAC_DRVR_LinkCheck( DRV_HANDLE hMac );

Returns

  • true - If the link is up
  • false - If the link is not up

Description

This function checks the link status of the associated network interface.

Remarks

The function will automatically perform a MAC reconfiguration if the link went up after being down and the PHY auto negotiation is enabled.

Preconditions

  • MAC_DRVR_Initialize() must have been called to set up the driver.
  • MAC_DRVR_Open() should have been called to obtain a valid handle.

Parameters

ParametersDescription
hMacEthernet MAC client handle