MAC_DRVR_Open Function
C
DRV_HANDLE MAC_DRVR_Open( const SYS_MODULE_INDEX drvIndex, const DRV_IO_INTENT intent );
Returns
- DRV_HANDLE - pointer to MAC client
- 0 if call failed
Description
This function opens a client instance of the PIC32 MAC Driver. Used by tcpip_module_manager.
Remarks
The intent parameter is not used in the current implementation and is maintained only for compatibility with the generic driver Open function signature.
Preconditions
MAC_DRVR_Initialize() should have been called.
Parameters
Parameters | Description |
---|---|
drvIndex | Identifier for the driver instance to be opened. |
intent | Zero or more of the values from the enumeration DRV_IO_INTENT ORed together to indicate the intended use of the driver |