MAC_DRVR_PowerMode Function
C
bool MAC_DRVR_PowerMode( DRV_HANDLE hMac, TCPIP_MAC_POWER_MODE pwrMode );
Returns
- true if the call succeeded.
- false if the call failed
Description
This function sets the power mode for the Ethernet MAC.
Remarks
This function is not currently supported by the Ethernet MAC and will always return true.
Preconditions
- MAC_DRVR_Initialize() must have been called to set up the driver.
- MAC_DRVR_Open() should have been called to obtain a valid handle.
Parameters
Parameters | Description |
---|---|
hMac | Ethernet MAC client handle |
pwrMode | Required power mode |