DRV_ETHMAC_PIC32MACStatisticsGet Function

C

TCPIP_MAC_RES DRV_ETHMAC_PIC32MACStatisticsGet(DRV_HANDLE hMac, TCPIP_MAC_RX_STATISTICS* pRxStatistics, TCPIP_MAC_TX_STATISTICS* pTxStatistics); 

Returns

  • TCPIP_MAC_RES_OK if all processing went on OK.
  • TCPIP_MAC_RES_OP_ERR error code if function not supported by the driver.

Description

This function will get the current value of the statistic counters maintained by the MAC driver.

Remarks

  • The reported values are info only and change dynamically.

Preconditions

DRV_ETHMAC_PIC32MACInitialize() should have been called. DRV_ETHMAC_PIC32MACOpen() should have been called to obtain a valid handle.