DRV_ETHMAC_PIC32MACLinkCheck Function
C
bool DRV_ETHMAC_PIC32MACLinkCheck(DRV_HANDLE hMac);
Returns
- true - If the link is up
- false - If the link is not up
Description
This function checks the link status of the associated network interface.
Remarks
The function will automatically perform a MAC reconfiguration if the link went up after being down and the PHY auto negotiation is enabled.
Preconditions
DRV_ETHMAC_PIC32MACInitialize must have been called to set up the driver. DRV_ETHMAC_PIC32MACOpen() should have been called to obtain a valid handle.
Parameters
Parameters | Description |
---|---|
hMac | Ethernet MAC client handle |