DRV_ETHMAC_PIC32MACOpen Function
C
DRV_HANDLE DRV_ETHMAC_PIC32MACOpen(const SYS_MODULE_INDEX drvIndex, const DRV_IO_INTENT intent);
Returns
- DRV_HANDLE - handle (pointer) to MAC client
- 0 if call failed
Description
This function opens a client instance of the PIC32 MAC Driver. Used by tcpip_module_manager.
Remarks
The intent parameter is not used in the current implementation and is maintained only for compatibility with the generic driver Open function signature.
Preconditions
DRV_ETHMAC_PIC32MACInitialize() should have been called.