DRV_ETHMAC_PIC32MACParametersGet Function

C

TCPIP_MAC_RES DRV_ETHMAC_PIC32MACParametersGet(DRV_HANDLE hMac, TCPIP_MAC_PARAMETERS* pMacParams); 

Returns

  • TCPIP_MAC_RES_OK if pMacParams updated properly
  • a TCPIP_MAC_RES error code if processing failed for some reason

Description

MAC Parameter Get function TCPIP_MAC_RES DRV_ETHMAC_PIC32MACParametersGet(DRV_HANDLE hMac, TCPIP_MAC_PARAMETERS* pMacParams); This is a function that returns the run time parameters of the MAC driver.

Remarks

None.

Preconditions

DRV_ETHMAC_PIC32MACInitialize() should have been called. DRV_ETHMAC_PIC32MACOpen() should have been called to obtain a valid handle.