DRV_ETHMAC_PIC32MACStatus Function
C
SYS_STATUS DRV_ETHMAC_PIC32MACStatus(SYS_MODULE_OBJ object);
Returns
- SYS_STATUS_READY - Indicates that any previous module operation for the specified module has completed
- SYS_STATUS_BUSY - Indicates that a previous module operation for the specified module has not yet completed
- SYS_STATUS_ERROR - Indicates that the specified module is in an error state
Description
This function provides the current status of the MAC driver module.
Remarks
None.
Preconditions
The DRV_ETHMAC_PIC32MACInitialize function must have been called before calling this function.
Parameters
Parameters | Description |
---|---|
object | Driver object handle, returned from DRV_ETHMAC_PIC32MACInitialize |