TCPIP_ANNOUNCE_FIELD_PAYLOAD Enumeration
C
typedef enum {
TCPIP_ANNOUNCE_FIELD_NONE = 0,
TCPIP_ANNOUNCE_FIELD_TRUNCATED,
TCPIP_ANNOUNCE_FIELD_MAC_ADDR,
TCPIP_ANNOUNCE_FIELD_MAC_NAME,
TCPIP_ANNOUNCE_FIELD_HOST_NAME,
TCPIP_ANNOUNCE_FIELD_IPV4_ADDRESS,
TCPIP_ANNOUNCE_FIELD_IPV6_UNICAST,
TCPIP_ANNOUNCE_FIELD_IPV6_MULTICAST,
TCPIP_ANNOUNCE_FIELD_IPV6_DEFAULT_ROUTER,
TCPIP_ANNOUNCE_FIELD_IPV6_DEFAULT_GATEWAY
} TCPIP_ANNOUNCE_FIELD_PAYLOAD;
Description
Enumeration: TCPIP_ANNOUNCE_FIELD_PAYLOAD - Describes the current types supported by the announce module payload.
Members
| Members | Description |
|---|---|
| TCPIP_ANNOUNCE_FIELD_NONE = 0 | invalid. |
| TCPIP_ANNOUNCE_FIELD_TRUNCATED | the payload is the truncated type. |
| TCPIP_ANNOUNCE_FIELD_MAC_ADDR | the payload is the MAC address. |
| TCPIP_ANNOUNCE_FIELD_MAC_NAME | the payload is the MAC name. |
| TCPIP_ANNOUNCE_FIELD_HOST_NAME | the payload is the host name. |
| TCPIP_ANNOUNCE_FIELD_IPV4_ADDRESS | the payload is the IPv4 address. |
| TCPIP_ANNOUNCE_FIELD_IPV6_UNICAST | the payload is the IPv6 unicast address. |
| TCPIP_ANNOUNCE_FIELD_IPV6_MULTICAST | the payload is the IPv6 multicast address. |
| TCPIP_ANNOUNCE_FIELD_IPV6_DEFAULT_ROUTER | the payload is the IPv6 router. |
| TCPIP_ANNOUNCE_FIELD_IPV6_DEFAULT_GATEWAY | the payload is the IPv6 gateway address. |