PPP_GetLocalIpv4Addr Function
C
uint32_t PPP_GetLocalIpv4Addr(DRV_HANDLE hMac);Returns
Current IPv4 local addressOr 0 if an error
Description
This function gets the PPP local IPv4 address currently assigned for the PPP driver
Remarks
This should be the IPv4 address passed at the PPP initializationIt could be a peer suggested address if the configuration address was 0or the peer suggested a different address.
Preconditions
The PPP module must be initialized.
Parameters
hMac - driver handle (obtained by calling TCPIP_MAC_Open/DRV_PPP_MAC_Open)