PPP_SendAdminEvent Function
C
bool PPP_SendAdminEvent(DRV_HANDLE hMac, PPP_EVENT event, PPP_CTRL_PROTO ctlProt);Returns
true - if the call succeeds
false - if the call failed (invalid handle)
Description
This function sends an administrative event to the PPP driver
Remarks
In normal operation just administrative PPP_EVENT_OPEN/PPP_EVENT_CLOSE events should be used
The event should be sent to LCP.An LCP PPP_EVENT_OPEN will eventually open IPCP too.An LCP PPP_EVENT_CLOSE will close IPCP too.
Sending events to IPCP is for testing purposes only and should not be normall used.
Preconditions
The PPP module must be initialized.
Parameters
hMac - driver handle (obtained by calling TCPIP_MAC_Open/DRV_PPP_MAC_Open)
event - event to be sent
ctlProt - the control protocol type: LCP or IPCP