PPP_EchoRequest Function
C
PPP_ECHO_RESULT PPP_EchoRequest (DRV_HANDLE hMac, PPP_ECHO_REQUEST* pEchoRequest, PPP_REQUEST_HANDLE* pHandle); Returns
PPP_ECHO_OK - Indicates the query request was successfully sent
PPP_ECHO_RESULT - The query request was unsuccessfully sent, which results in an error code (interface not ready for transmission, allocation error, etc.)
Description
This function allows a PPP client to send an PPP query message to a peer. The request will also contain user supplied data. The request is scheduled and the user will be notified of the outcome of the query using the callback function that's specified in the call.
Remarks
The data buffer that's passed as part of the callback routine is no longer available after the callback routine returns control.
The number of active echo requests at a time is controlled by PPP_MAX_ECHO_REQUESTS. If more requests are active, a PPP_ECHO_BUSY code will be returned.
Once the callback notification occurs, the echo request is completed and the pppHandle is invalidated.
Preconditions
The IP PPP module initialized and up and running.
Parameters
hMac - driver handle (obtained by calling TCPIP_MAC_Open/DRV_PPP_MAC_Open)
pEchoRequest - pointer to a PPP_ECHO_REQUEST data structure describing the request:
pData - data buffer in the request
dataSize - number of bytes in the data buffer
callback - callback function to be called when a reply is received
pHandle - address to store a handle to this PPP request.
It will contain a valid handle/pointer if the call succeeded, 0 otherwise.
It can be used to cancel the request (if the user timeout is < than the PPP timeout: PPP_ECHO_REQUEST_TIMEOUT) Could be NULL if not needed.
Example
uint8_t myDataBuffer[200]; // buffer for the echo request data
void EchoCallback(PPP_ECHO_REQUEST* pReqData, PPP_REQUEST_HANDLE pppHandle, PPP_ECHO_RESULT result); // callback function to be called
PPP_ECHO_REQUEST myEchoRequest;
myEchoRequest.pData = myDataBuffer;
myEchoRequest.dataSize = sizeof(myDataBuffer);
myEchoRequest.callback = EchoCallback;
if(PPP_EchoRequest(hMac, &myEchoRequest, 0) == PPP_ECHO_OK )
{
// successfully sent the PPP request
//
// EchoCallback() will be called and data can be examined
}
else
{
// process the error
}