TCPIP_TFTPS_Enable Function
C
bool TCPIP_TFTPS_Enable(TCPIP_NET_HANDLE hNet, IP_ADDRESS_TYPE ipType); Returns
true - if successful
false - if unsuccessful, if server open fails for this interface.
Description
This function enables the TFTP server for the specified interface and it opens the TFTP server with specific IP address TYPE.
Remarks
None.
Preconditions
The TFTPS module should have been initialized.
Parameters
| Parameters | Description |
|---|---|
| hNet | Interface to enable |
| ipType | Interface address type. Depends on the enum type of IP_ADDRESS_TYPE bool TCPIP_TFTPS_Enable( TCPIP_NET_HANDLE hNet,IP_ADDRESS_TYPE ipType) |