TCPIP_TFTPS_Disable Function
C
bool TCPIP_TFTPS_Disable(TCPIP_NET_HANDLE hNet); Returns
true - if successful
false - if unsuccessful
Description
This function disables the TFTP server for the specified interface.
Remarks
None.
Preconditions
The TFTPS module should have been initialized.
Parameters
| Parameters | Description |
|---|---|
| hNet | Interface for which to disable. |