DRV_ETHMAC_PIC32MACReinitialize Function
C
void DRV_ETHMAC_PIC32MACReinitialize(SYS_MODULE_OBJ object, const SYS_MODULE_INIT * const init); Returns
None.
Description
This function supports re-initialization of the PIC32 Ethernet MAC (opposite of set up).
Remarks
This function is not supported yet.
Preconditions
DRV_ETHMAC_PIC32MACInitialize must have been called to set up the driver.
Example Function
void DRV_ETHMAC_PIC32MACReinitialize(SYS_MODULE_OBJ object, const SYS_MODULE_INIT * const init);