TCPIP_DHCPS_CLIENT_OPTION_CONFIG Structure
C
typedef struct
{
TCPIP_DHCPS_CLIENT_OPTION_TYPE optType;
union
{
const char* ipStr;
uint32_t uintVal;
struct
{
uint16_t mult;
uint16_t div;
};
};
}TCPIP_DHCPS_CLIENT_OPTION_CONFIG;
Description
Structure: TCPIP_DHCPS_CLIENT_OPTION_CONFIG
DHCP server configuration of client options
DHCP server configuration of provided client options Lists the options to be presented to clients requiring an address lease
Remarks
An option is allowed to appear multiple times. For example, using TCPIP_DHCPS_CLIENT_OPTION_DNS 2 times, 2 DN servers will be communicated to the client
The maximum number of values possible for an option is dictated by: TCPIP_DHCPS_OPTION_ROUTER_VALUESTCPIP_DHCPS_OPTION_DNS_VALUESTCPIP_DHCPS_OPTION_TIME_SERVER_VALUES TCPIP_DHCPS_OPTION_NAME_SERVER_VALUES TCPIP_DHCPS_OPTION_NTP_SERVER_VALUES
Excess values will be ignored.
Members
| Members | Description |
|---|---|
| optType | Option type |
| ipStr | a string describing the option, a valid IP address string |
| used for TCPIP_DHCPS_CLIENT_OPTION_ROUTER, TCPIP_DHCPS_CLIENT_OPTION_DNS, TCPIP_DHCPS_CLIENT_OPTION_TIME_SERVER, | |
| TCPIP_DHCPS_CLIENT_OPTION_NAME_SERVER, TCPIP_DHCPS_CLIENT_OPTION_NTP_SERVER | |
| uintVal | a uint32_t value |
| mult, div | uint16_t values |
| used for TCPIP_DHCPS_CLIENT_OPTION_T1_RENEWAL and TCPIP_DHCPS_CLIENT_OPTION_T2_REBINDING | |
| the T1 and T2 are obtained as percentages of lease time: | |
| T1 = (leaseTime * mult) / div; default values are mult = 1, div = 2; | |
| T2 = (leaseTime * mult) / div; default values are mult = 7, div = 8; | |
| Default values are used for mult or div if any of them are 0 | |
| T2 needs to be greater than T1! |