PPP_EventHandlerDeregister Function
C
bool PPP_EventHandlerDeregister(DRV_HANDLE hMac, PPP_EVENT_HANDLE hPPP);
Returns
true - if the call succeeds
false - if no such handler is registered
Description
This function deregisters the PPP event handler.
Remarks
This API exists only when the build symbol PPP_NOTIFICATIONS_ENABLE != 0
Preconditions
The PPP module must be initialized.
Parameters
hMac - driver handle (obtained by calling TCPIP_MAC_Open/DRV_PPP_MAC_Open)
hPPP - A handle returned by a previous call to PPP_EventHandlerRegister.