PPP_StatHandlerRegister Function
C
PPP_STAT_HANDLE PPP_StatHandlerRegister(DRV_HANDLE hMac, PPP_STAT_HANDLER handler);
Returns
Returns a valid handle if the call succeeds, or a null handle if the call failed (out of memory, for example).
Description
This function registers a PPP statistics handler.
The PPP module will call the registered handler when a PPP statistics increment occurs.
Remarks
The handler has to be short and fast. It is meant for setting an event flag, not for lengthy processing!
This API exists only when the build symbol PPP_ENABLE_STATISTICS != 0
Preconditions
The PPP module must be initialized.
Parameters
hMac - driver handle (obtained by calling TCPIP_MAC_Open/DRV_PPP_MAC_Open)
handler - Handler to be called when a PPP statistics occurs.