PPP_GetRemoteIpv4Addr Function

C

uint32_t PPP_GetRemoteIpv4Addr(DRV_HANDLE hMac);

Returns

Current IPv4 remote addressOr 0 if an error

Description

This function gets the PPP remote IPv4 address currently assigned for the PPP driver

Remarks

This is the IPv4 address of the remote nodeIt is set during PPP negotiation

It could be a suggested address by this node (not supported yet)

Preconditions

The PPP module must be initialized.

Parameters

hMac - driver handle (obtained by calling TCPIP_MAC_Open/DRV_PPP_MAC_Open)