gethostbyname Function
C
struct hostent * gethostbyname(
char * name
);
Preconditions
None.
Parameters
Parameters | Description |
---|---|
name | The name of the host to be found. |
Returns
The hostent structure if function is successful.
NULL if there is an error.
Remarks
This function supports IPv4 only. h_errno will be set to:
TRY_AGAIN if the DNS query is currently in progress.
HOST_NOT_FOUND if the DNS query could not find a host name.
NO_RECOVERY if the DNS query had an unrecoverable error.