setsockopt Function
C
int setsockopt(
SOCKET s,
uint32_t level,
uint32_t option_name,
const uint8_t * option_value,
uint32_t option_length
);
Description
Various options can be set at the socket level. This function provides compatibility with BSD implementations.
Preconditions
None.
Parameters
Parameters | Description |
---|---|
s | Socket descriptor returned from a previous call to socket. |
level | On which level the operation is to be performed: - IPPROTO_IP: applies to the IP protocol layer (not yet supported). - IPPROTO_TCP: applies to the TCP protocol layer. - SOL_SOCKET: applies to the socket layer. - IPPROTO_IPV6: applies to the IPv6 protocol layer (not yet supported). - IPPROTO_ICMPV6: applies to the ICMPv6 protocol layer (not yet supported). |
option_name | The name of the option to be set: -IPPROTO_TCP -TCP_NODELAY: specifies whether or not the stack should use the Nagle algorithm. - SOL_SOCKET - SO_LINGER: specifies what the stack should do with unsent data on close(). - SO_RCVBUF: specifies the size of the receive buffer (TCP only). - SO_SNDBUF: specifies the size of the transmit buffer. |
option_value | For all values of option_name, this is a pointer to the data, which in most cases is an integer. The only exception is SO_LINGER which points to a linger structure. |
option_length | The size of the data pointed to by option_value. |
Returns
0 - If the function is successful.
-1 - If the function is unsuccessful.
Remarks
None.