10.3.4.1 Output Section .reset
On dsPIC33C/E/F architectures, section .reset contains a GOTO instruction, created at link time, from output section
data commands:
/*
** Reset Instruction
*/
.reset __RESET_BASE :
{
SHORT(ABSOLUTE(__reset));
SHORT(0x04);
SHORT((ABSOLUTE(__reset) >> 16) & 0x7F);
SHORT(0);
} >reset
Each SHORT() data command causes a 2
byte value to be included. There are two expressions which include the symbol __reset, which by convention is the first function invoked
after a device reset. Each expression calculates a portion of the address of the Reset
function. These declarations encode a GOTO instruction,
which is two instruction words long.
The ABSOLUTE() function specifies the final value of a program symbol after linking. If this function were omitted, a relative (before-linking) value of the program symbol would be used.
The >reset portion of this definition indicates that this section should be allocated in the Reset memory region.
On dsPIC33A architectures, section .reset contains a vector (address) that points to the
location of symbol __reset, which by convention is the first function
invoked after a device reset.
/*
** Reset Vector
*/
.reset :
{
LONG(ABSOLUTE(__reset));
} >reset
The LONG() data command causes a 4 byte value to be included.
The ABSOLUTE() function specifies the final value of a program symbol
after linking. If this function were omitted, a relative (before-linking) value of the
program symbol would be used.
The >reset portion of this definition indicates that this section should
be allocated in the Reset memory region.