3 Kit Setup
Perform the following steps to set up the ATAK51005-V1 kit:
- On the ATSAMC21-XPRO microcontroller board, ensure that the VCC-SEL jumper is set to the 5.0V position.
- If using the ATA5291-XPRO board,
perform the following actions; otherwise, skip to step 3.
- Insert the ATA5291-XPRO LF coil driver/immobilizer board in the EXT3 connector on the ATSAMC21-XPRO board.
- Connect the ATAB-LFTX LF antenna module to Ant0 on the ATA5291-XPRO board.
- Ensure that the J1 jumper
on the LF antenna module is set to the inductor only (
) position, and go to step 4.
Note: For use of the antenna on the Ant1-7 connectors, ensure that the jumper on the LF antenna module is set to the LCR position.
- If using the ATA5293-XPRO,
perform the following actions:
- Insert the ATA5293-XPRO LF coil driver/immobilizer board in the EXT3 connector on the ATSAMC21-XPRO board.
- Connect the X-10013-002 antenna to Ant0 on the ATA5293-XPRO board.Note: For use of the Ant1-5 and 8 connectors, the X-10013-003 antenna is required.
Figure 3-1. ATAK51005-V1 Kit Setup - Insert the ATA5831-XPRO RF transceiver board in the EXT1 connector on the ATSAMC21-XPRO board.
- Connect the UHF SMA whip antenna to the ATA5831-XPRO board at the ANT2 SMA connector.
- If UWB functionality is being
evaluated, perform the following actions; otherwise, skip to step 7.
- Insert the ATA8352-XPRO UWB transceiver board in the EXT2 connector on the ATSAMC21-XPRO board.
- Connect the UWB PCB antenna to the ATA8352-XPRO board.
- Connect the UWB board to the EXT2 connector on ATAB5702A fob board.
- Connect the UWB PCB antenna to the UWB XPRO board.
- Connect the 12V DC power supply to the power socket (J11) on the ATA5291-XPRO board using the DC plug adapter cable.
Note:
- Always unplug the adapter cable and the USB cable prior to inserting or removing any boards within the system.
- Always remove the battery from the fob board prior to inserting or removing any boards.