6 Programming Instructions
Specific firmware (Flash) and, in some devices, configuration settings (EEPROM) are required to
operate the system. These are found in the MCU (ATSAMC21-XPRO) and the RF transceiver
(ATA5831-XPRO) on the vehicle side. The fob requires its own PEPS, IMMO and RKE firmware
and configuration files. The following list describes exactly what type of files are
needed for each device:
- Vehicle side:
- ATSAMC21-XPRO: PEPS, IMMO and RKE firmware and configuration in Flash
- ATA5831-XPRO: PEPS and RKE configuration in the EEPROM
- Fob side:
- ATAB5702A fob board: PEPS, IMMO and RKE firmware in Flash and configuration in the EEPROM
Note: All devices within this system are
shipped unprogrammed; therefore, the programming procedure is described in the following
sections. Programming is also required when the revised ATAK51005-V1 tool package
software is available for download from www.microchip.com/developmenttools/ProductDetails/ATAK51005-V1 or when the source code has been modified or when a device
becomes erratic or unresponsive in behavior.