9.2.18 __fpnormalize Function
A function that normalizes a floating-point value.
Include
<xc.h>
Prototype
__fpnormalize(double value);
value- The floating-point value to normalize
Remarks
This function can be used to ensure that an arbitrary 32-bit floating-point value (which is not the result of a calculation performed by the compiler) conforms to the "relaxed" floating-point rules (as described in Section 4.4.4 “Floating-Point Data Types”).
This function returns the value passed to it, but ensures that any subnormal argument is flushed to zero, and converts any negative zero argument to a positive zero result.
Example
#include <xc.h>
int main(void)
{
double input_fp;
// read in a floating-point value from an external source
input_fp = getFP();
// ensure it is formatted using the relaxed rules
input_fp = __fpnormalize(input_fp);
}