9.2.10 _delaywdt Builtin
A builtin function that delays execution.
Include
<xc.h>
Prototype
void _delaywdt(unsigned long cycles);
Argument
cycles- The number of cycles to delay
Remarks
This is an inbuilt function that is expanded by the code generator. When called, this routine expands to an in-line assembly delay sequence. The sequence will consist of code that delays for the number of instruction cycles that is specified as the argument. The argument must be a constant expression that does not contain variables or function calls and that can be fully evaluated at compile time.
The _delay() builtin function can use loops and the
clrwdt instruction to implement the delay.
An error will result if the requested delay is not a constant expression or is greater than 50,463,240 instructions. For even larger delays, call this function multiple times.
Example
All of the inbuilt delay routines are shown in the following example.
#include <xc.h>
/* _XTAL_FREQ is defined by MCC headers; when not using MCC, place a definition similar to:
#define _XTAL_FREQ 4000000
in your code to ensure that the 'us' and 'ms' forms of delay routines work as expected. */
unsigned char count;
void main(void) {
SYSTEM_Initialize();
while (1) {
LATA = 0xFF;
_delay(100); /* wait 100 cycles*/
LATA = 0xAA;
_delaywdt(100); /* wait 100 cycles, clearing the watchdog */
LATA = 0x55;
_delay3(10); /* wait 30 cycles */
LATA = 0xFF;
__delay_us(800); /* wait 800 micro seconds */
LATA = 0x00;
__delaywdt_us(800); /* wait 800 micro seconds, clearing the watchdog */
LATA = count;
__delay_ms(500); /* wait half a second */
LATA = ~count;
__delaywdt_ms(500); /* wait half a second, clearing the watchdog */
count++;
}
}