5.8.1.3 Reentrant And Nonreentrant Specifiers
The __reentrant and __nonreentrant
function specifiers indicate the function model that should be used for that function’s
stack-based variables (auto and parameters), as shown in the Table 5-11 table. The aliases __software and
__compiled, respectively, can be used if you prefer. You would only use
these specifiers if the default allocation is unacceptable.
| Specifier | Allocation for Stack-based variables |
|---|---|
__compiled,
__nonreentrant | Always use the compiled stack; functions are nonreentrant |
__software,
__reentrant | Use the software or register-optimized reentrant stack, if available; functions are reentrant |
The following shows an example of a function that will always be encoded as reentrant.
__reentrant int setWriteMode(int mode)
{
accessMode = (mode!=0);
retrun mode;
}These specifiers override any setting indicated using the
-mstack option (see Stack Option). If neither function
specifier is used with a function and the -mstack option is not specified
(or specified as hybrid), then the compiler will choose the stack to be used by that
function for its stack-based variables.
The __reentrant specifier only has an effect if the
target device supports a software or register-optimized reentrant stack. In addition, not
all functions allow reentrancy. Interrupt functions must always use the compiled stack, but
functions they call may use the software stack. Functions encoded for Baseline and
Mid-range devices always use the nonreentrant model and the compiled stack.
Repeated use of the __software
(__reentrant) specifier might increase substantially the size of the
software stack leading to possible overflow. The size of the software stack is not
accurately known at compile time, so the compiler cannot issue a warning if it is likely to
overwrite memory used for some other purpose.
See Data Stacks for device specific information relating to the data stacks available on each device.