6.1.1.7 Long Jumps And Calls
The assembler recognizes several mnemonics that expand into regular PIC MCU assembly instructions. The mnemonics are
fcall and ljmp.
On baseline and mid-range parts, these instructions expand into regular
call and goto instructions respectively, but also
ensure the instructions necessary to set the bits in PCLATH (for mid-range devices) or
STATUS (for baseline devices) will be generated, should the destination be in another page
of program memory. Page selection instructions can appear immediately before the
call or goto, or be generated as part of, and
immediately after, a previous fcall/ljmp mnemonic.
On PIC18 devices, these mnemonics are present purely for compatibility
with smaller 8-bit devices and are always expanded as regular PIC18 call
and goto instructions.
These special mnemonics should be used where
possible, as they make assembly code independent of the final position of the routines that
are to be executed. Whether the page selection instructions are generated, and exactly
where they will be located, is dependent on the surrounding source code. If the
call or goto is determined to be within the current
page, the additional code to set the PCLATH bits can be optimized away.
The operand to the fcall and ljmp mnemonics should not be
masked, regardless of target device. The full address is required to determine the
destination address and page (where applicable). When the mnemonic is expanded, the address
used with either the call or goto instruction in the
expansion will be automatically masked. When using a call or
goto instruction directly in your source code, always apply the
appropriate mask to the operand.
The following mid-range PIC example shows an fcall
instruction in the assembly list file. You can see that the fcall
instruction has expanded to five instructions. In this example, there are two bit
instructions that set/clear bits in the PCLATH register. Bits are also set/cleared in this
register after the call to reselect the page that was selected before the
fcall.
13 0079 3021 movlw 33
14 007A 120A 158A 2000 fcall _phantom
120A 118A
15 007F 3400 retlw 0
Since fcall and ljmp instructions can
expand into more than one instruction, they should never be preceded by an instruction that
can skip, e.g., a btfsc instruction.
The fcall and ljmp instructions assume
that the psect that contains them is smaller than a page. Do not use these instructions to
transfer control to a label in the current psect if it is larger than a page. The default
linker options will not permit code psects to be larger than a page.
On PIC18 devices, the regular call instruction can be
followed by a “,f” to indicate that the W, STATUS and BSR registers should
be pushed to their respective shadow registers. This replaces the “,1”
syntax indicated on the device data sheet.