3.6.1.5 Const-data-in-progmem Option
The -mconst-data-in-progmem option changes the location
of where objects defined using just the const type qualifier are
stored.
By default, all objects defined using just the const
type qualifier are located in and accessed from program memory, and this action can be
made explicit by using the -mconst-data-in-progmem option. Any pointer
to a const-qualified object will be able to read both data and program
memory and determine at runtime which space is to be accessed. See also Objects in Program Space.
The -mno-const-data-in-progmem option forces all objects defined using
just the const type qualifier to be copied to data memory, where they
can be read using different instructions when required. Disabling this feature does not
affect code built for devices that have flash mapped into data memory, for example the
avrxmega3 and avrtiny architectures. Pointers to objects qualified with just
const will always read from data memory, and alternatives to the
string functions normally provided by <string.h> must be used to
access strings that have been located in program memory.
The macro __AVR_CONST_DATA_IN_PROGMEM__ is defined if this feature is
enabled and const-qualified objects are located in and accessed from
program memory.
Having const-qualified objects in program memory will
free up more valuable RAM and does not require the use of non-standard keywords, making
it easier to have pointers access such objects. Accessing
const-qualified objects in data memory is the more efficient in terms
of program size.