3.6.1.12 Relax Option
The -mrelax option enables several optimizations that
relate to the efficient use of call and jump instructions.
These optimizations include replacement of the long-form call and jump instructions with
shorter and/or faster relative calls and jumps when the relative forms of the
instructions can be determined to be in range of their destination. For example, code
such as:
call foo
...
foo:
...can be replaced with: rcall foo
...
foo:
...when foo is within range of the relative call. (For
more information, see Function Pointers).When relative calls would be out of range, the compiler will attempt to replace them with
rcall instructions to a jmp instruction that will
'trampoline' execution to the required address. For example, code such
as: call foo
...
call foo
...
call foocan be changed
to: rcall tramp_foo
...
rcall tramp_foo
...
rcall tramp_foo
...
tramp_foo:
jmp fooprovided the trampoline is within range of the relative calls. The
compiler will re-use an existing jmp instruction to the required
destination if possible, to further reduce code size. Such transformations will slow
execution speed but can improve code size if there multiple calls that can be
replaced.Additionally, redundant return instructions are removed from functions with a tail call.
For example, code such as:
...
call last
return
last:
...
returncan be replaced with: ...
jmp last
last:
...
returnThe -mno-relax form of this option does not apply these optimizations
and is the default action if no option is specified.