2.10 Reset Line
As part of checking if the target cable is correctly mounted it will, after VTARGET is applied, check if the reset line has the correct voltage and check if it is possible to force this line low.
If there is no pull-up resistor on the line, i.e. if the Atmel AVRISP mkII detects 0V on reset, then the status LED will blink orange.
If the pull-up resistor on the reset line is too strong, the short circuit protection will trigger when the reset is forced low by the AVRISP mkII.
The Reset line should not have a pull-up stronger (i.e. smaller value) than 4.7kΩ. Any decoupling capacitor should not be larger than 10μF. No decoupling capacitor can be present for PDI programming (refer to XMEGA® Schematic Checklist).
The AT89 devices that are supported by AVRISP mkII has the opposite reset polarity. If the AVRISP mkII has been used with a Atmel AVR and then connected to a AT89, it may start to blink orange indicating error on reset. When AT89 is selected in the programming dialog and e.g. Read Signature is performed the orange blinking will occur. The same applies to the opposite situation where AT89 is used before an AVR.