5.10.2.3 Monitor Aggregation LACP Neighbor Status
The LACP Neighbor Status page provides a status overview for the LACP neighbor status for all ports. Only ports that are part of an LACP group are shown. For details on the shown parameters, see the IEEE 801.AX-2014.
The LACP Neighbor Status page has the following parameters:
- Port: The switch port number
- State: The current port
state:
- Down: The port is not active
- Active: The port is in active state
- Standby: The port is in standby state
- Aggr ID: The aggregation group ID which the port is assigned to
- Partner Key: The key assigned to this port by the partner
- Partner Port: The partner port number associated with this link
- Partner Port Priority: The priority assigned to this partner port
- Activity: The LACP mode of the group (Active or Passive)
- Timeout: The timeout mode configured for the partner port (Fast or Slow)
- Aggregation: Show whether the partner considers this link to be aggregateable; that is, a potential candidate for aggregation.
- Synchronization: Shows whether the partner considers this link to be IN_SYNC; that is, it has been allocated to the correct LAG, the group has been associated with a compatible Aggregator, and the identity of the LAG is consistent with the System ID and operational Key information transmitted.
- Collecting: Shows if collection of incoming frames on this link is enabled
- Distributing: Shows if distribution of outgoing frames on this link is enabled
- Defaulted: Shows if the partners Receive machine is using Defaulted operational Partner information
- Expired: Shows if that the partners Receive machine is in the EXPIRED state