7.6.1 Options Specific to 16-Bit Devices
For more information on the memory models, see section Memory Models.
| Option | Definition |
|---|---|
-mcodecov | This option is used for MPLAB® Code Coverage support.
Passing the option -mcodecov=near or
-mcodecov=far to the compiler causes it to
instrument the generated assembly-instruction blocks with information
that the MPLAB X IDE can then use to perform a code coverage analysis.
This feature requires MPLAB X IDE v5.25 or later. For more on this
features, visit: |
-mconst-in-code | Put const qualified
variables in the auto_psv space. The compiler will
access these variables using the PSV window (This is the
default). |
-mconst-in-data | Put const qualified
variables in the data memory space. |
-mconst-in-
auxflash | When combined with
-mconst-in-code, put all const
qualified file scope variables into auxiliary Flash. All modules with
auxiliary Flash should be compiled with this option; otherwise a link
error may occur. |
-mcpu=
target | This option selects the target
processor ID (and communicates it to the assembler and linker if those
tools are invoked). This option affects how some predefined constants
are set; see section Predefined Macro Names for
more information. A full list of accepted targets can be seen in the
Readme.htm file that came with the release. |
-mdfp=path | This option directs the compiler to use the device support included in the specified device family pack (DFP). The directory should be to the 'xc16' folder within the pack. This option is usually used by MPLAB X IDE or MPLAB IPE when specifying a pack. |
-mno-eds-warn | On some devices, there is a possibility
that the stack will reside in EDS (extended data space) memory (above
0x8000), though this allocation is disabled by default in the linker. If
the stack is located in this area, then taking the address of an auto
variable would require an __eds__ pointer. As the
compiler does not know where the stack will be located, the default is
to be conservative and warn if the address of an auto is taken and not
used as an __eds__ pointer. This option disables the
warning. |
-merrata=
id[,id]* | This option enables specific errata
workarounds identified by id. Valid values for
id change from time to time and may not be required for a particular
variant. An id of list will
display the currently supported errata identifiers along with a brief
description of the errata. An id of
all will enable all currently supported errata
workarounds. |
-mno-errata=
id[,id]* | This option disables specific errata
workarounds identified by id. Valid values for
id change from time to time. This is
particularly useful when specifying errata with
-merrata=all as it can be used to disable some
errata that are not required. -mno-errata=foo will
prevent the erratum foo from being enabled no matter
where it appears on the command line. Therefore, -mno-errata=foo
-merrata=foo will not enable erratum
foo. |
-mno-file | Do not emit a .file
directive in the generated assembly file. This is useful when creating
libraries where the source code may not reside on the end-user's
machine, as this will prevent the IDE from trying to load the source
file during a debug session. |
-mfillupper | Specify the upper byte of variables
stored into space(prog) sections. The
fillupper attribute will perform the same function
on individual variables. |
-mlarge-arrays | Specifies that arrays may be greater than or equal to the default maximum size of 32K. See Non-Auto Variable Allocation and Access, Non-Auto Variable Size Limits for more information. |
-mlarge-code | Compile using the large code model. No
assumptions are made about the locality of called functions. When this option is chosen, single functions that are larger than 32k are not supported and may cause assembly-time errors since all branches inside of a function are of the short form. |
-mlarge-data | Compile using the large data model. No assumptions are made about the location of static and external variables. |
-mlegacy-libc | MPLAB XC16 (originally MPLAB C30) has a long history. This option allows us to support previously deployed C libraries as needed (This is the default). |
-moptimize-page
-setting | Attempt to reduce the number page switches when using memory modes that affect the PSVPAG. This is really an optimization, and is not enabled by default. Like all optimizations it will generally have a positive effect on performance or code size. |
-mpa1. | Enable the procedure abstraction
optimization. There is no limit on the nesting level. Optimization levels depend on the compiler edition (see section Optimizations). |
-mpa=n1. | Enable the procedure abstraction
optimization up to level n. If
n is zero, the optimization is
disabled. If n is 1, first level of
abstraction is allowed; that is, instruction sequences in the source
code may be abstracted into a subroutine. If
n is 2, a second level of
abstraction is allowed; that is, instructions that were put into a
subroutine in the first level may be abstracted into a subroutine one
level deeper. This pattern continues for larger values of
n. The net effect is to limit
the subroutine call nesting depth to a maximum of
n.Optimization levels depend on the compiler edition (see Optimizations). |
-mno-pa1. | Do not enable the procedure abstraction optimization (This is the default). |
-mpreserve-all | Make all variables in this translation unit preserved unless explicitly marked with the update attribute. |
-mprint-
builtins | Display the complete list of target builtin functions available in the compiler. |
-mprint-devices | Display the complete list of real and virtual devices supported by the current installation. |
-mprint-mchp-
search-dirs | A target-specific option to output the compiler and assembler include search paths to the console. These paths can change based upon various options. |
-mno-isr-warn | By default the compiler will produce a
warning if the __interrupt__ is not attached to a
recognized interrupt vector name. This option will disable that
feature. |
-omf | Selects the OMF (Object Module Format)
to be used by the compiler. The omf specifier can be
one of the following:
The debugging format used for ELF object files is DWARF 2.0. |
-msfr-warn | By default we warn when accessing SFRs
for a generic device; use -mno-sfr-warn to disable this
feature. |
-msmall-code | Compile using the small code model. Called functions are assumed to be proximate (within 32 Kwords of the caller). (This is the default.) |
-msmall-data | Compile using the small data model. All static and external variables are assumed to be located in the lower 8 KB of data memory space. (This is the default.) |
-msmall-scalar | Like -msmall-data,
except that only static and external scalars are assumed to be in the
lower 8 KB of data memory space. (This is the default.) |
-msmart-io-
format=fmt | When using smart-io the compiler is not
able to detect the format string when it is a variable.
-msmart-io-format can be used to tell the compiler
which format specifiers to expect in such a string. For example:
can be compiled with
|
-mtext=name | Specifying
-mtext=name will cause text
(program code) to be placed in a section named
name rather than the default
.text section. No white spaces should appear around
the =. |
-mauxflash | Place all code from the current translation unit into auxiliary Flash. This option is only available on devices that have auxiliary Flash. |
-msmart-io
[=0|1|2] | This option attempts to statically
analyze format strings passed to printf,
scanf and the ‘f’ and ‘v’ variations of these
functions. Uses of nonfloating point format arguments will be converted
to use an integer-only variation of the library functions.
|
--partition
n | This option targets a single partition
n in a dual partition device and will constrain the
output text to be contained within one panel. |
Note 1: The procedure abstractor
behaves as the inverse of inlining functions. The pass is designed to
extract common code sequences from multiple sites throughout a
translation unit and place them into a common area of code. Although
this option generally does not improve the run-time performance of the
generated code, it can reduce the code size significantly. Programs
compiled with -mpa can be harder to debug; it is not
recommended that this option be used while debugging using the COFF
object format.
The procedure abstractor is invoked as a separate phase
of compilation, after the production of an assembly file. This phase
does not optimize across translation units. When the
procedure-optimizing phase is enabled, inline assembly code must be
limited to valid machine instructions. Invalid machine instructions or
instruction sequences, or assembler directives (sectioning directives,
macros, include files, etc.), must not be used, or the procedure
abstraction phase will fail, inhibiting the creation of an output
file. | |