7.6.12 Miscellaneous Options
The following options do not fit in any of the previous categories.
| Option | Definition |
|---|---|
--nofallback | By default, the tool will fall back to a free license when a network,
or other license, is unavailable. Specifying this option will prevent fallback and cause the compilation to fail instead. |
-v | Print the commands executed during each stage of compilation. |
-x | You can specify the input language explicitly with the
-x option:-x language Specify
explicitly the language for the following input files (rather than
letting the compiler choose a default based on the file name
suffix). This option applies to all following input files until the
next The following values are supported by the compiler:
-x none Turn off
any specification of a language, so that subsequent files are
handled according to their file name suffixes. This is the default
behavior but is needed if another For example:
Without
the |