7.6.9 Options for Linking
If any of the options -c, -S or
-E are used, the linker is not run and object file names should not
be used as arguments. For more on available options, see the MPLAB®
XC16 Assembler, Linker and Utilities User’s Guide (DS50002106).
| Option | Definition |
|---|---|
--fill=options | Fill unused program memory. The format
is:
A single value
Range of values
An incrementing value
By default, the linker will fill using data that is
instruction-word length. For 16-bit devices, the default fill width
is 24 bits. However, you may specify the value width using Multiple fill options may be specified on the command line; the linker will always process fill options at specific locations first. |
--gc-sections | Remove dead functions from code at link
time. Support is for ELF projects only. In order
to make the best use of this feature, add the
|
-Ldir | Add directory
dir to the list of directories to be
searched for libraries specified by the command-line option
-l. |
-legacy-libc | Use legacy include files and libraries
(v3.24 and before). The format of include file and libraries changed in v3.25 to match HI-TECH C compiler format. |
-llibrary | Search the library named
library when linking.The linker searches a standard list of directories for the library,
which is actually a file named It makes a difference where in the
command you write this option; the linker processes libraries and
object files in the order they are specified. Thus, The directories searched include
several standard system directories, plus any that you specify with
Normally the files
found this way are library files (archive files whose members are
object files). The linker handles an archive file by scanning
through it for members which define symbols that have so far been
referenced but not defined. But if the file that is found is an
ordinary object file, it is linked in the usual fashion. The only
difference between using an By default the linker is directed to search:
for libraries specified with the
This behavior can be overridden using the environment variables defined in the Predefined Macro Names section. |
-nodefaultlibs | Do not use the standard system
libraries when linking. Only the libraries you specify will be passed to
the linker. The compiler may generate calls to memcmp,
memset and memcpy. These entries
are usually resolved by entries in the standard compiler libraries.
These entry points should be supplied through some other mechanism when
this option is specified. |
-nostdlib | Do not use the standard system startup
files or libraries when linking. No startup files and only the libraries
you specify will be passed to the linker.
The compiler may generate
calls to memcmp, memset and
memcpy. These entries are usually resolved by
entries in standard compiler libraries. These entry points should be
supplied through some other mechanism when this option is
specified. |
-s | Remove all symbol table and relocation information from the executable. |
-T
script | Specify the linker script file,
script, to be used at link time. This
option is translated into the equivalent -T linker
option. |
-u symbol | Pretend symbol
is undefined to force linking of library modules to define the symbol.
It is legitimate to use -u multiple times with
different symbols to force loading of additional library
modules. |
-Wl,option | Pass option as
an option to the linker. If option contains
commas, it is split into multiple options at the commas.For example, to generate a map file, use
|
-Xlinker
option | Pass option as
an option to the linker. You can use this to supply system-specific
linker options that the compiler does not know how to recognize. |