11.3.4.3 ISR Considerations [DD]
A data access using managed PSV pointers is definitely not atomic, meaning it can take several instructions to complete the access. Care should be taken if an access should not be interrupted.
Furthermore an Interrupt Service Routine (ISR) never really knows what
the current state of the PSVPAG register will be. Unfortunately the
compiler is not really in any position to determine whether or not this is important in
all cases.
The compiler will make the simplifying assumption that the writer of the
interrupt service routine will know whether or not the automatic, compiler managed
PSVPAG is required by the ISR. This is required to access any
constant data in the auto_psv space or any string literals or constants
when the default -mconst-in-code option is selected. When defining an
interrupt service routine, it is best to specify whether or not it is necessary to
assert the default setting of the PSVPAG SFR.
This is achieved by adding a further attribute to the interrupt function definition:
auto_psv- the compiler will set thePSVPAGregister to the correct value for accessing theauto_psvspace, ensuring that it is restored when exiting the ISRno_auto_psv- the compiler will not set thePSVPAGregister
For example:
void __attribute__((interrupt, no_auto_psv)) _T1Interrupt(void) {
IFS0bits.T1IF = 0;
}
The choice is provided so that, if you are especially conscious of
interrupt latency, you may select the best option. Saving and setting the
PSVPAG will consume approximately 3 cycles at the entry to the
function and one further cycle to restore the setting upon exit from the function.