11.3.4.2 Object Compatibility Model [DD]
Since functions in secure segments set PSVPAG to their respective
psv constant sections, a convention must be established for
managing multiple values of the PSVPAG register. In previous versions of the compiler, a
single value of PSVPAG was set during program startup if the default
constants-in-code memory model was selected. The compiler relied
upon that preset value for accessing const variables and string
literals, as well as any variables specifically nominated with
space(auto_psv).
MPLAB XC-DSC provides support for multiple
values of PSVPAG. Variables declared with
space(auto_psv) may be combined with secure segment constant
variables and/or managed psv variables in the same source file.
Precompiled objects that assume a single, pre-set value of PSVPAG are
link-compatible with objects that define secure segment psv constants
or managed psv variables.
Even though PSVPAG is considered to be a
compiler-managed resource, there is no change to the function calling conventions.