4.3.5.8 Where are Arguments That Are Passed to Functions Located in Memory?
You will need to run compiler code to determine this. See the application binary interface when running the compiler. Some built-ins may also be helpful. See the following location of this user’s guide: