22.3.2.4.4.9 Input Mode 9: Stop Output at Level, Maintain Frequency
In Input mode 9 a positive edge on the input Event while the corresponding output is on will cause the output to stop during the rest of the on-time. The TCD counter will not be affected by the Event, only the output.
If Input mode 9 is used on input A and an positive input Event occurs while in On time A, the output will be off for the rest of the on-time.
If Input mode 9 is used on input B and an positive input event occurs while in On time B, the output will be off for the rest of the on-time.