ATT error codes
C
#define ATT_ERR_INVALID_HANDLE 0x01 #define ATT_ERR_READ_NOT_PERMITTED 0x02 #define ATT_ERR_WRITE_NOT_PERMITTED 0x03 #define ATT_ERR_INVALID_PDU 0x04 #define ATT_ERR_INSUF_AUTHN 0x05 #define ATT_ERR_REQUEST_NOT_SUPPORT 0x06 #define ATT_ERR_INVALID_OFFSET 0x07 #define ATT_ERR_INSUF_AUTHZ 0x08 #define ATT_ERR_PREPARE_QUEUE_FULL 0x09 #define ATT_ERR_ATTRIBUTE_NOT_FOUND 0x0a #define ATT_ERR_ATTRIBUTE_NOT_LONG 0x0b #define ATT_ERR_INSUF_ENC_KEY_SIZE 0x0c #define ATT_ERR_INVALID_ATTRIBUTE_VALUE_LENGTH 0x0d #define ATT_ERR_UNLIKELY_ERROR 0x0e #define ATT_ERR_INSUF_ENC 0x0f #define ATT_ERR_UNSUPPORTED_GROUP_TYPE 0x10 #define ATT_ERR_INSUF_RESOURCE 0x11 #define ATT_ERR_DATABASE_OUT_OF_SYNC 0x12 #define ATT_ERR_VALUE_NOT_ALLOW 0x13 #define ATT_ERR_APPLICATION_ERROR 0x80
Description
Defines ATT (Attribute Protocol) error codes used in BLE communication.
Macro Definition
| Macro | Description |
|---|---|
| ATT_ERR_INVALID_HANDLE | Error Code: The attribute handle given was not valid on this server. |
| ATT_ERR_READ_NOT_PERMITTED | Error Code: The attribute cannot be read. |
| ATT_ERR_WRITE_NOT_PERMITTED | Error Code: The attribute cannot be written. |
| ATT_ERR_INVALID_PDU | Error Code: The attribute PDU was invalid. |
| ATT_ERR_INSUF_AUTHN | Error Code: The attribute requires authentication before it can be read or written. |
| ATT_ERR_REQUEST_NOT_SUPPORT | Error Code: Attribute server does not support the request received from the client. |
| ATT_ERR_INVALID_OFFSET | Error Code: Offset specified was past the end of the attribute. |
| ATT_ERR_INSUF_AUTHZ | Error Code: The attribute requires authorization before it can be read or written. |
| ATT_ERR_PREPARE_QUEUE_FULL | Error Code: Too many prepare writes have been queued. |
| ATT_ERR_ATTRIBUTE_NOT_FOUND | Error Code: No attribute found within the given attribute handle range. |
| ATT_ERR_ATTRIBUTE_NOT_LONG | Error Code: The attribute cannot be read or written using the Read Blob Request. |
| ATT_ERR_INSUF_ENC_KEY_SIZE | Error Code: The Encryption Key Size used for encrypting this link is insufficient. |
| ATT_ERR_INVALID_ATTRIBUTE_VALUE_LENGTH | Error Code: The attribute value length is invalid for the operation. |
| ATT_ERR_UNLIKELY_ERROR | Error Code: The attribute request that was requested has encountered an error that was unlikely, and therefore could not be completed as requested. |
| ATT_ERR_INSUF_ENC | Error Code: The attribute request that was requested has encountered an error that was unlikely, and therefore could not be completed as requested. |
| ATT_ERR_UNSUPPORTED_GROUP_TYPE | Error Code: The attribute type is not a supported grouping attribute as defined by a higher layer specification. |
| ATT_ERR_INSUF_RESOURCE | Error Code: Insufficient Resources to complete the request. |
| ATT_ERR_DATABASE_OUT_OF_SYNC | Error Code: The server requires the client to rediscover the database. |
| ATT_ERR_VALUE_NOT_ALLOW | Error Code: The attribute value is not allowed. |
| ATT_ERR_APPLICATION_ERROR | Error Code: The application has set this error code. |