Attribute settings
C
#define SETTING_MANUAL_WRITE_RSP 0x01 #define SETTING_MANUAL_READ_RSP 0x02 #define SETTING_UUID_16 0x04 #define SETTING_VARIABLE_LEN 0x08 #define SETTING_ALLOW_OFFSET 0x10 #define SETTING_CCCD 0x20
Description
Defines the attribute settings.
Macro Definition
| Macro | Description |
|---|---|
| SETTING_MANUAL_WRITE_RSP | Set if the service needs to be informed of write operations on this attribute. The service also needs to send a response manually if required. |
| SETTING_MANUAL_READ_RSP | Set if the service needs to be informed of read operations on this attribute. The service also needs to send a response manually. |
| SETTING_UUID_16 | Set if the UUID is 16 bytes (128 bits) in length. |
| SETTING_VARIABLE_LEN | Set if the attribute has a variable length value. |
| SETTING_ALLOW_OFFSET | Set if the attribute allows write operations with an offset. |
| SETTING_CCCD | Set if the attribute is a Client Characteristic Configuration Descriptor (CCCD). |