2.3 Memory Verification Selector
This component is used to set the verification method used for application
verification.
Description: Verification of the application image is a vital part to any bootloading process. This component allows users to configure the verification scheme that will be used by the bootloader to verify the presence or validity of the application image. Some of these methods can also perform checks on the integrity and authenticity of the application image. For more information about the specific verification schemes, refer to the Verification Schemes section.