2.1 Communication Protocol
This component is used to configure which communication protocol is being used for data
transfer between the Bootloader and the Host application.
Description: This component was added into the bootloader UI to give users the ability to select any of the supported protocols for enabling communication between the bootloader code and the host application. Supported protocols will include UART, USART, and EUSART.
Example: There are two main steps to configuring a communication interface for the
bootloader. Simply click anywhere in the Communication Protocol box to see a drop down
menu with all the options currently available for the bootloader. Select the protocol and
attach the specific driver version from that module’s MCC tab. For more information on the
setup step for this option, refer to the Use Case Examples
section.