1.23 PIT Start Stop
This example application shows how PIT can be started and stopped at run time.
Description
Pushing the user switch will stop/start the PIT counter, which in turn stops/starts the LED toggling.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/pit/start_stop/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_a5d29_curiosity.X | MPLABX project for SAMA5D29 Curiosity Development Board Kit |
Setting Up AT91Bootstrap Loader
To load the application binary onto the target device, we need to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_a5d29_curiosity.X | SAMA5D29 Curiosity Development Board Kit |
Setting Up SAMA5D29 Curiosity Development Board
- Connect the Debug USB port on the board to the computer using a Type-C USB cable
Running the Application
- Build the application using its IDE
- Press the switch to start toggling the LED
- Press the switch again to stop toggling the LED
| Board | Switch Name | LED Name |
|---|---|---|
| SAMA5D29 Curiosity Development Board | USER | RGB_LED (Blue) |