1.39 TWIHS EEPROM Emulation
This example application demonstrates how to use the TWIHS peripheral in Slave mode.
Description
This example uses the TWIHS peripheral library in Slave mode and emulates an EEPROM of 512 bytes. There are two pages each of size 256 bytes. TWIHS Slave expects two bytes of memory address from the TWIHS Master and the memory address can range from 0x00 to 0x1FF. TWIHS Slave application supports following:
Byte Write: The TWIHS Master sends the Slave address, followed by two bytes of memory address. The Slave provides the data present at the requested memory address.
Page Write: A page write is initiated the same way as a byte write, but the TWIHS Master can write up-to 256 bytes (1 page). If more than 256 bytes are sent by the TWIHS Master to the TWIHS Slave, the memory address will “roll over” and previous data will be overwritten. The address “roll over” during write is from the last byte of the current page to the first byte of the same page.
Current Address Read: The internal memory address counter maintains the last address accessed during the last read or write operation, incremented by one. Once the device address with the read/write bit set to one is clocked in and acknowledged by the EEPROM, the data byte at the current address is serially clocked out. After reading the data from the current address, the TWIHS Master sends NAK and generates a STOP condition.
Random Read: The TWIHS Master writes the 2 byte memory address and then reads the data from that memory address. After reading the data, the TWIHS Master sends NAK and generates a STOP condition.
Sequential Read: Sequential reads are initiated by either a current address read or a random address read. As long as the EEPROM receives an acknowledge, it will continue to increment the memory address and serially clock out sequential data bytes. When the memory address limit is reached (0x1FF), the memory address will “roll over” to 0x00 and the sequential read will continue. The sequential read operation is terminated when the TWIHS Master sends a NAK and generates a STOP condition.
To run the application, two evaluation kits will be required - one acting as the TWIHS Master and the other as the TWIHS Slave. The TWIHS Master application to be used for this demo application is available under apps/twihs/master/twihs_eeprom/firmware folder. TWIHS Master writes an array of values to the TWIHS Slave and verifies the value written by reading the values back and comparing it to the value written.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/twihs/slave/i2c_eeprom_emulation/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_a5d29_curiosity.X | MPLABX project for SAMA5D29 Curiosity Development Board Kit |
Setting Up AT91Bootstrap Loader
To load the application binary onto the target device, we need to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_a5d29_curiosity.X | SAMA5D29 Curiosity Development Board Kit |
Hardware setup requires two boards, one acting as the TWIHS Master and the other as the TWIHS Slave.
Setting Up SAMA5D29 Curiosity Development Board
- Connect the Debug USB port on the board to the computer using a Type-C USB cable
- Connect TWIHS SDA line on Pin 11 (PD4) of J19 connector and TWIHS SCL line on Pin 12 (PD5) with the corresponding SDA and SCL lines of the TWIHS master. Refer the TWIHS master documentation for connection details.
- Connect a ground wire between TWIHS Master and TWIHS Slave boards
Running the Application
- Open the twihs_eeprom application
from apps/twihs/master/twihs_master_write_read/firmware and open the
main.c file. Make sure the following macro is defined to
false.
#define I2C_SLAVE_IS_ONBOARD_EEPROM falseBuild twihs_eeprom application (which is used as TWIHS Master) using its IDE
- Build TWIHS Slave application (used as TWIHS Slave) using its IDE
- Run application on TWIHS Slave board and then run the application on TWIHS Master board
- LED on the TWIHS Master board
indicates success or failure:
- The LED is turned ON when the value read from the TWIHS Slave matches with the written value
- The LED is turned OFF when the value read from the TWIHS Slave did not match with the written value