1.20 MCAN Interrupt

This example application shows how to use the MCAN module to transmit and receive CAN messages in Interrupt mode.

Description

This application transmits and receives CAN messages on the CAN bus. To run this application, two evaluation boards of same type are required. These boards acts as different nodes on the CAN bus. Same application is programmed onto both the boards. Boards are connected to PC via UART. While running the application, user can send and receive CAN messages between the boards using UART console applications running on the PC.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/mcan/mcan_normal_operation_interrupt/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
sam_a5d29_curiosity.XMPLAB X project for SAMA5D29 Curiosity Development Board Kit

Setting Up AT91Bootstrap Loader

To load the application binary onto the target device, the user needs to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
sam_a5d29_curiosity.XSAMA5D29 Curiosity Development Board Kit

Setting Up SAMA5D29 Curiosity Development Board

ADDITIONAL HARDWARE REQUIRED
SETTING UP THE BOARD
  • Connect two ATA6563 Click boards using female to female DB9 serial cable
  • Connect each ATA6563 Click board to SAMA5D29 Curiosity board as per the pin connections shown below
    SAMA5D9 Curiosity BoardATA6563 Click Board
    CANTX0 (Pin 4), mikroBUS 1 connectorRX (Pin 13)
    CANTX0 (Pin 4), mikroBUS 1 connectorTX (Pin 14)
    3V3 (Pin 20), mikroBUS 1 connector3V3 (Pin 7)
    VDD_5V (Pin 3), mikroBUS 1 connector5V (Pin 10)
    GND (Pin 19), mikroBUS 1 connectorGND (Pin 8)
  • Connect the UART Debug port on the board to the computer using a FTDI to USB cable
  • Connect the Debug USB port on the board to the computer using a USB Type-C cable

Running the Application

  1. Build the application using its IDE.
  2. Open the Terminal application (e.g., Tera term) on the computer.
  3. Connect to the Virtual COM port and configure the serial settings as follows:
    • Baud: 115200
    • Data: 8 Bits
    • Parity: None
    • Stop: 1 Bit
    • Flow Control: None
  4. Build and Program the application on both the boards using the respective IDEs.
  5. In the console associated with board 1, press '1' to transmit a CAN message.
  6. Transmitted message status will be displayed in the console window of board 1.
  7. Received message will be displayed in the console window of board 2.
  8. Follow the sequence below to send and receive CAN message:
    • Press '1' on board 2
  9. If the steps are executed in this sequence, the final output in the consoles will be as below.