1.47 USART Ring Buffer
This example application shows how to use USART peripheral in Ring buffer mode.
Description
This example demonstrates read and write over USART using the Ring buffer mode. The USART is configured in Non-blocking mode (interrupts enabled). The example asks the user to enter 10 characters. Once received, the characters are echoed back. In the process, the example demonstrates various ring buffer APIs.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/uart/uart_ring_buffer_interrupt/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_a5d29_curiosity.X | MPLAB X project for SAMA5D29 Curiosity Development Board Kit |
| sam_a5d27_som1_ek.X | MPLAB X project for SAMA5D27-SOM1-EK1 |
| sam_a5d27_wlsom1_ek1.X | MPLAB X project for ATSAMA5D27-WLSOM1 Evaluation Kit |
Setting Up AT91Bootstrap Loader
To load the application binary onto the target device, the user needs to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_a5d29_curiosity.X | SAMA5D29 Curiosity Development Board |
| sam_a5d27_som1_ek.X | SAMA5D27-SOM1-EK1 |
| sam_a5d27_wlsom1_ek1.X | ATSAMA5D27-WLSOM1 Evaluation Kit |
Setting Up SAMA5D29 Curiosity Development Board Kit
- Connect UART Debug port on the board to the computer using a FTDI USB cable
- Connect the Debug USB port on the board to the computer using a USB Type-C cable
Setting Up SAMA5D27-SOM1-EK1
- Connecting a micro-USB cable to J10 both powers the board as well as provides a virtual COM port to open a serial terminal
Setting Up ATSAMA5D27-WLSOM1 Evaluation Kit
- Connect a USB to UART FTDI cable to J26 (DEBUG FTDI) to open a serial terminal
- Connecting a micro-USB cable to J10 powers the board
- Press the SW3 (nSTART_SOM) button to power the ATSAMA5D27-WLSOM1 System-On-Module
Running the Application
- Build the application using its IDE.
- Open the Terminal application (e.g., Tera term) on the computer.
- Connect to the EDBG/J-link
Virtual COM port and configure the serial settings as follows:
- Baud: 115200
- Data: 8 Bits
- Parity: None
- Stop: 1 Bit
- Flow Control: None
- The console displays the
following message.

- The console displays the initial transmit and receive buffer sizes
- It then adds 10 characters, 0123456789, to the transmit buffer and displays the available free space in the transmit buffer after the 10 characters have been added
- The message asks the user
to enter 10 charactersNote: For this example, the “Free Space in Transmit Buffer = xx”, where xx can be anything between 117 to 127, depending on the USART baud rate and the CPU execution speed.
- Enter 10 characters on the terminal.
- Entered characters are echoed
back on the console and message is displayed indicating that the receive
notification is turned on.

- For every 10 characters typed, it
will be echoed back on the console.