1.25 PIT Polling
This example application shows how to use PIT counter in Polling mode.
Description
This example application configures the PIT Peripheral Library in Polling mode and it enables PIT counter. Whenever PIT time period expires then LED toggles and then PIT counter restarts again.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/pit/led_toggle_polling/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_a5d29_curiosity.X | MPLAB X project for SAMA5D29 Curiosity Development Board Kit |
Setting Up AT91Bootstrap Loader
To load the application binary onto the target device, the user needs to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_a5d29_curiosity.X | SAMA5D29 Curiosity Development Board Kit |
Setting Up SAMA5D29 Curiosity Development Board
- Connect the Debug USB port on the board to the computer using a USB Type-C cable
Running the Application
- Build the application using its IDE.
- LED toggles every 1 second.
| Board | LED Name |
|---|---|
| SAMA5D29 Curiosity Development Board | RGB_LED (Blue) |